This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:text:chapter-9 [26 Feb 2017 13:48] – [9.7.2 BJT Version DC Biasing techniques] Jack Liu | university:courses:electronics:text:chapter-9 [06 Jun 2017 17:26] – [9.3.4 Output impedance, current follower or common base/gate amplifier] Doug Mercer | ||
---|---|---|---|
Line 125: | Line 125: | ||
====9.2.5 common emitter and source Lab Activities==== | ====9.2.5 common emitter and source Lab Activities==== | ||
- | [[university: | + | **ADALM1000 Lab Activity 5, [[university: |
- | [[university: | + | **ADALM1000 Lab Activity 5M, [[university: |
- | [[university: | + | |
+ | **ADALM2000 Lab Activity 5, [[university: | ||
+ | **ADALM2000 Lab Activity 5M, [[university: | ||
+ | **ADALM2000 Lab Activity 5FR, [[university: | ||
=====9.3 The Current Follower also known as Common base or gate amplifier===== | =====9.3 The Current Follower also known as Common base or gate amplifier===== | ||
Line 168: | Line 171: | ||
Again looking at the small signal models in figure 9.3.1 we see that for both the BJT case and the MOS case the output impedance is the parallel combination of R< | Again looking at the small signal models in figure 9.3.1 we see that for both the BJT case and the MOS case the output impedance is the parallel combination of R< | ||
+ | **ADALM1000 Lab Activity, [[university: | ||
+ | **ADALM1000 Lab Activity, [[university: | ||
+ | **ADALM1000 Lab Activity, [[university: | ||
==== 9.4 Voltage followers (also called Emitter or Source follower or Common collector or drain amplifiers) ==== | ==== 9.4 Voltage followers (also called Emitter or Source follower or Common collector or drain amplifiers) ==== | ||
Line 225: | Line 231: | ||
====9.4.5 Voltage Follower (common collector or drain) Lab Activities ==== | ====9.4.5 Voltage Follower (common collector or drain) Lab Activities ==== | ||
- | [[university: | + | **ADALM1000 Lab Activity 11, [[university: |
- | [[university: | + | **ADALM1000 Lab Activity 11M, [[university: |
+ | **ADALM2000 Lab Activity 11, [[university: | ||
+ | **ADALM2000 Lab Activity 11m, [[university: | ||
=====9.5 Series Feedback: emitter/ | =====9.5 Series Feedback: emitter/ |