Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Next revision Both sides next revision
university:courses:electronics:text:chapter-9 [26 Feb 2017 13:48]
JackZL [9.7.2 BJT Version DC Biasing techniques]
university:courses:electronics:text:chapter-9 [06 Jun 2017 17:26]
dmercer [9.3.4 Output impedance, current follower or common base/gate amplifier]
Line 125: Line 125:
 ====9.2.5 common emitter and source Lab Activities==== ====9.2.5 common emitter and source Lab Activities====
  
-[[university:​courses:​electronics:​electronics-lab-5|Common emitter amplifier]]\\ +**ADALM1000 Lab Activity 5, [[university:​courses:​alm1k:​alm-lab-5|Common emitter amplifier]]**\\ 
-[[university:​courses:​electronics:​electronics-lab-5m|Common source amplifier]]\\ +**ADALM1000 Lab Activity 5M, [[university:​courses:​alm1k:​alm-lab-5m|Common source amplifier]]** 
-[[university:​courses:​electronics:​electronics-lab-5fr|Amplifier Frequency Response]]+ 
 +**ADALM2000 Lab Activity 5, [[university:​courses:​electronics:​electronics-lab-5|Common emitter amplifier]]**\\ 
 +**ADALM2000 Lab Activity 5M, [[university:​courses:​electronics:​electronics-lab-5m|Common source amplifier]]**\\ 
 +**ADALM2000 Lab Activity 5FR, [[university:​courses:​electronics:​electronics-lab-5fr|Amplifier Frequency Response]]**
  
 =====9.3 The Current Follower also known as Common base or gate amplifier===== =====9.3 The Current Follower also known as Common base or gate amplifier=====
Line 168: Line 171:
 Again looking at the small signal models in figure 9.3.1 we see that for both the BJT case and the MOS case the output impedance is the parallel combination of R<​sub>​L</​sub>​ and r<​sub>​o</​sub>​. We can generally assume this is true if we consider that V<​sub>​in</​sub>​ is driven from a low impedance (nearly ideal) voltage source. If this is not the case then the finite output impedance must be added in series with r<​sub>​o</​sub>​. If the input of the current follower is driven by the relatively high output impedance of a transconductance amplifier such as the common emitter or source amplifier from earlier then the output impedance for the combined amplifier can be very high. For most practical applications we can ignore r<​sub>​o</​sub>​ because it is very often much larger than R<​sub>​L</​sub>​. ​ Again looking at the small signal models in figure 9.3.1 we see that for both the BJT case and the MOS case the output impedance is the parallel combination of R<​sub>​L</​sub>​ and r<​sub>​o</​sub>​. We can generally assume this is true if we consider that V<​sub>​in</​sub>​ is driven from a low impedance (nearly ideal) voltage source. If this is not the case then the finite output impedance must be added in series with r<​sub>​o</​sub>​. If the input of the current follower is driven by the relatively high output impedance of a transconductance amplifier such as the common emitter or source amplifier from earlier then the output impedance for the combined amplifier can be very high. For most practical applications we can ignore r<​sub>​o</​sub>​ because it is very often much larger than R<​sub>​L</​sub>​. ​
  
 +**ADALM1000 Lab Activity, [[university:​courses:​alm1k:​alm-lab-cb|BJT Common Base Amplifier]]**\\
 +**ADALM1000 Lab Activity, [[university:​courses:​alm1k:​alm-lab-cg|BJT Common Gate Amplifier]]**\\
 +**ADALM1000 Lab Activity, [[university:​courses:​alm1k:​alm-lab-fca|Folded Cascode Amplifier]]**
 ==== 9.4 Voltage followers (also called Emitter or Source follower or Common collector or drain amplifiers) ==== ==== 9.4 Voltage followers (also called Emitter or Source follower or Common collector or drain amplifiers) ====
  
Line 225: Line 231:
 ====9.4.5 Voltage Follower (common collector or drain) Lab Activities ==== ====9.4.5 Voltage Follower (common collector or drain) Lab Activities ====
  
-[[university:​courses:​electronics:electronics-lab-11|BJT Emitter follower]]\\ +**ADALM1000 Lab Activity 11, [[university:​courses:​alm1k:alm-lab-11|BJT Emitter follower]]**\\ 
-[[university:​courses:​electronics:electronics-lab-11m|MOS ​source ​follower]]\\+**ADALM1000 Lab Activity 11M, [[university:​courses:​alm1k:alm-lab-11m|MOS ​Source ​follower]]**
  
 +**ADALM2000 Lab Activity 11, [[university:​courses:​electronics:​electronics-lab-11|BJT Emitter follower]]**\\
 +**ADALM2000 Lab Activity 11m, [[university:​courses:​electronics:​electronics-lab-11m|MOS Source follower]]**
  
 =====9.5 Series Feedback: emitter/​source degeneration===== =====9.5 Series Feedback: emitter/​source degeneration=====
university/courses/electronics/text/chapter-9.txt · Last modified: 03 May 2019 16:33 by dmercer