This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:text:chapter-6 [31 Jan 2014 16:31] – [6.1.2 Full-wave rectification] Doug Mercer | university:courses:electronics:text:chapter-6 [06 Jun 2017 17:03] (current) – [Regulator Design Example:] Doug Mercer | ||
---|---|---|---|
Line 39: | Line 39: | ||
<WRAP centeralign > Figure 6.4 Dual polarity Full-wave rectifier using a center tapped transformer and 4 diodes. </ | <WRAP centeralign > Figure 6.4 Dual polarity Full-wave rectifier using a center tapped transformer and 4 diodes. </ | ||
+ | |||
+ | **ALM1000 Lab Activity [[: | ||
====6.1.3 Rectifier output smoothing==== | ====6.1.3 Rectifier output smoothing==== | ||
Line 137: | Line 139: | ||
The maximum power that could be dissipated in the zener when there is zero current in the output load can be calculated as P< | The maximum power that could be dissipated in the zener when there is zero current in the output load can be calculated as P< | ||
- | ** Lab Activity: [[university: | + | **ADALM2000 |
**Exercise 6.3.1** | **Exercise 6.3.1** |