This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:text:chapter-6 [01 Sep 2013 15:08] – [Regulator Design Example:] Doug Mercer | university:courses:electronics:text:chapter-6 [31 Jan 2014 16:31] – [6.1.2 Full-wave rectification] Doug Mercer | ||
---|---|---|---|
Line 20: | Line 20: | ||
==== 6.1.2 Full-wave rectification==== | ==== 6.1.2 Full-wave rectification==== | ||
- | A full-wave rectifier converts both the positive and negative halves of the input waveform to a single polarity (positive or negative) at its output. By using both halves of the AC waveform full-wave rectification is more efficient than half wave. However, in a circuit | + | A full-wave rectifier converts both the positive and negative halves of the input waveform to a single polarity (positive or negative) at its output. By using both halves of the AC waveform full-wave rectification is more efficient than half wave. |
+ | |||
+ | When a simple transformer | ||
{{ : | {{ : |