This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:courses:electronics:text:chapter-3 [06 Jun 2017 16:47] – [3.2.4 Frequency Dependence of Loop Gain] Doug Mercer | university:courses:electronics:text:chapter-3 [06 Jun 2017 16:49] (current) – [3.2.3 Loop gain] Doug Mercer | ||
---|---|---|---|
Line 89: | Line 89: | ||
This loop gain discussion emphasizes that indeed, loop gain is a very significant factor in predicting the performance of closed-loop operational amplifier circuits. The open-loop gain required to obtain an adequate amount of loop gain will, of course, depend on the desired closed-loop gain. | This loop gain discussion emphasizes that indeed, loop gain is a very significant factor in predicting the performance of closed-loop operational amplifier circuits. The open-loop gain required to obtain an adequate amount of loop gain will, of course, depend on the desired closed-loop gain. | ||
- | For example, using equation 3-9, an amplifier with A< | + | For example, using equation 3-9, an amplifier with A< |
+ | |||
+ | **ADALM1000 Lab Activity [[university: | ||
====3.2.4 Frequency Dependence of Loop Gain ==== | ====3.2.4 Frequency Dependence of Loop Gain ==== |