Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
university:courses:electronics:text:chapter-2 [06 Aug 2014 13:23] – minor edit Doug Mercer | university:courses:electronics:text:chapter-2 [06 Jun 2017 16:44] – [2.8 The Differential Op Amp Stage] Doug Mercer |
---|
If all the input resistors R<sub>1</sub>, R<sub>2</sub>, ... R<sub>n</sub> are equal but not equal to R<sub>f</sub> then from the equation we can see that it can be simplified such that the output will be equal to the algebraic sum of the inputs times a common gain factor of -R<sub>f</sub>/R<sub>1</sub>. If all the resistors are made equal including R<sub>f</sub> then the output will be simply the negative sum of the inputs. | If all the input resistors R<sub>1</sub>, R<sub>2</sub>, ... R<sub>n</sub> are equal but not equal to R<sub>f</sub> then from the equation we can see that it can be simplified such that the output will be equal to the algebraic sum of the inputs times a common gain factor of -R<sub>f</sub>/R<sub>1</sub>. If all the resistors are made equal including R<sub>f</sub> then the output will be simply the negative sum of the inputs. |
| |
**Lab Activity 1. [[university:courses:electronics:electronics-lab-1|Simple Op Amps]]** | **ADALM1000 Lab Activity 1. [[university:courses:alm1k:alm-lab-1|Simple Op Amps]]**\\ |
| **ADALM2000 Lab Activity 1. [[university:courses:electronics:electronics-lab-1|Simple Op Amps]]**\\ |
| **ADALM2000 Lab Activity [[university:courses:alm1k:alm-lab-vectrosumamp|Summing Amplifier]]** |
| |
=====2.8 The Differential Op Amp Stage ===== | =====2.8 The Differential Op Amp Stage ===== |
<WRAP centeralign> Figure 2.8.1: Buffered differential amplifier stage </WRAP> | <WRAP centeralign> Figure 2.8.1: Buffered differential amplifier stage </WRAP> |
| |
| **ADALM1000 Lab Activity [[university:courses:alm1k:alm-lab-diffamp|Difference Amplifier]]**\\ |
| **ADALM1000 Lab Activity [[university:courses:alm1k:alm-lab-current-sense|Current Sensing Difference Amplifier]]** |
=====2.9 The Instrumentation Amplifier===== | =====2.9 The Instrumentation Amplifier===== |
| |