Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision Both sides next revision
university:courses:electronics:text:chapter-2 [06 Aug 2014 13:23]
Doug Mercer minor edit
university:courses:electronics:text:chapter-2 [06 Jun 2017 16:37]
Doug Mercer [2.7 Inverting Summing Op Amp Stage]
Line 136: Line 136:
 If all the input resistors R<​sub>​1</​sub>,​ R<​sub>​2</​sub>,​ ... R<​sub>​n</​sub>​ are equal but not equal to R<​sub>​f</​sub>​ then from the equation we can see that it can be simplified such that the output will be equal to the algebraic sum of the inputs times a common gain factor of -R<​sub>​f</​sub>/​R<​sub>​1</​sub>​. If all the resistors are made equal including R<​sub>​f</​sub>​ then the output will be simply the negative sum of the inputs. If all the input resistors R<​sub>​1</​sub>,​ R<​sub>​2</​sub>,​ ... R<​sub>​n</​sub>​ are equal but not equal to R<​sub>​f</​sub>​ then from the equation we can see that it can be simplified such that the output will be equal to the algebraic sum of the inputs times a common gain factor of -R<​sub>​f</​sub>/​R<​sub>​1</​sub>​. If all the resistors are made equal including R<​sub>​f</​sub>​ then the output will be simply the negative sum of the inputs.
  
-**Lab Activity 1. [[university:​courses:​electronics:​electronics-lab-1|Simple Op Amps]]**+**ADALM1000 Lab Activity 1. [[university:​courses:​alm1k:​alm-lab-1|Simple Op Amps]]**\\ 
 +**ADALM2000 ​Lab Activity 1. [[university:​courses:​electronics:​electronics-lab-1|Simple Op Amps]]**
  
 =====2.8 The Differential Op Amp Stage  ===== =====2.8 The Differential Op Amp Stage  =====
university/courses/electronics/text/chapter-2.txt · Last modified: 06 Jun 2017 16:44 by Doug Mercer