This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:text:chapter-2 [31 Aug 2013 16:26] – [2: Introduction and Chapter Objectives] Doug Mercer | university:courses:electronics:text:chapter-2 [06 Jun 2017 16:37] – [2.7 Inverting Summing Op Amp Stage] Doug Mercer | ||
---|---|---|---|
Line 80: | Line 80: | ||
However, if the values of the resistors are too low, a great deal of current is required from the op amp output for proper operation. This causes excessive power dissipation in the op amp itself, which has many disadvantages. The increased dissipation leads to self-heating of the integrated circuit, which can cause a change in the dc characteristics of the op amp itself. | However, if the values of the resistors are too low, a great deal of current is required from the op amp output for proper operation. This causes excessive power dissipation in the op amp itself, which has many disadvantages. The increased dissipation leads to self-heating of the integrated circuit, which can cause a change in the dc characteristics of the op amp itself. | ||
- | From a practical sense, resistors below 10 ? and above 1 M? are more difficult to produce, especially if precision resistors are required. | + | From a practical sense, resistors below 10 Ω and above 1 MegΩ are more difficult to produce, especially if precision resistors are required. |
=====2.5 Inverting Op Amp Gain Derivation ===== | =====2.5 Inverting Op Amp Gain Derivation ===== | ||
Line 136: | Line 136: | ||
If all the input resistors R< | If all the input resistors R< | ||
- | **Lab Activity 1. [[university: | + | **ADALM1000 Lab Activity 1. [[university: |
+ | **ADALM2000 | ||
=====2.8 The Differential Op Amp Stage ===== | =====2.8 The Differential Op Amp Stage ===== |