Next revision Both sides next revision
university:courses:electronics:text:chapter-2 [29 Aug 2013 20:28]
Doug Mercer [2.10.2 The Ideal Differentiator]
university:courses:electronics:text:chapter-2 [06 Aug 2014 13:23]
Doug Mercer minor edit
Line 1: Line 1:
-======2: ​ Introduction and Chapter Objectives======+======Chapter ​2: Introduction and Chapter Objectives======
  
 =====2.1 The Ideal Voltage Feedback Op Amp ===== =====2.1 The Ideal Voltage Feedback Op Amp =====
Line 80: Line 80:
 However, if the values of the resistors are too low, a great deal of current is required from the op amp output for proper operation. This causes excessive power dissipation in the op amp itself, which has many disadvantages. The increased dissipation leads to self-heating of the integrated circuit, which can cause a change in the dc characteristics of the op amp itself. ​ Also, the heat generated can eventually cause the junction temperature to rise above 150º C, the commonly accepted maximum limit for most semiconductors. The junction temperature is the temperature at the silicon chip itself. On the other end of the spectrum, if the resistor values are too high, there is an increase in noise and the susceptibility to parasitic capacitances,​ which can limit bandwidth and possibly cause instability and oscillation. ​   ​ However, if the values of the resistors are too low, a great deal of current is required from the op amp output for proper operation. This causes excessive power dissipation in the op amp itself, which has many disadvantages. The increased dissipation leads to self-heating of the integrated circuit, which can cause a change in the dc characteristics of the op amp itself. ​ Also, the heat generated can eventually cause the junction temperature to rise above 150º C, the commonly accepted maximum limit for most semiconductors. The junction temperature is the temperature at the silicon chip itself. On the other end of the spectrum, if the resistor values are too high, there is an increase in noise and the susceptibility to parasitic capacitances,​ which can limit bandwidth and possibly cause instability and oscillation. ​   ​
    
-From a practical sense, resistors below 10 and above 1 M? are more difficult to produce, especially if precision resistors are required. ​+From a practical sense, resistors below 10 Ω and above 1 MegΩ are more difficult to produce, especially if precision resistors are required. ​
    
 =====2.5 Inverting Op Amp Gain Derivation ===== =====2.5 Inverting Op Amp Gain Derivation =====
university/courses/electronics/text/chapter-2.txt · Last modified: 06 Jun 2017 16:44 by Doug Mercer