This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:courses:electronics:text:chapter-14 [29 Sep 2013 20:51] – [14.3 Bandgap References] Doug Mercer | university:courses:electronics:text:chapter-14 [06 Jun 2017 17:55] (current) – [14.3 Bandgap References] Doug Mercer | ||
---|---|---|---|
Line 311: | Line 311: | ||
output tolerances as low as 0.4%, with TCs as low as 10 ppm/°C. | output tolerances as low as 0.4%, with TCs as low as 10 ppm/°C. | ||
- | **Bandgap reference [[university: | + | **ADALM1000 Lab Activity 9, [[university: |
- | **Shunt Bbandgap reference | + | **ADALM1000 Lab Activity 10, [[university: |
+ | |||
+ | **ADALM2000 Lab Activity 9, [[university: | ||
+ | **ADALM2000 Lab Activity 10, [[university: | ||
=====14.4 Buried (sub-surface) Zener References===== | =====14.4 Buried (sub-surface) Zener References===== |