Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (06 Mar 2018 16:48) was approved by Antoniu Miclaus.The Previously approved version (06 Mar 2018 14:31) is available.Diff

This is an old revision of the document!


Activity: Temperature Control using Window Comparator

Objective

The objective of this lab activity is to use two high speed voltage comparators as a Window-Comparator and program the TMP01 Low Power Programmable Temperature Controller using this approach.

A Window-Comparator is a circuit configuration, usually consisting of a pair of voltage comparators (inverting and non-inverting), in which the output indicates whether an input signal is within the voltage range bounded by two different thresholds. One which triggers an op-amp comparator on detection of some upper voltage threshold, VREF(HIGH) and one which triggers an op-amp comparator on detection of a lower voltage threshold level, VREF(LOW). The voltage levels between these two upper and lower reference voltages is called the “window”.

Materials

ADALM2000 Active Learning Module
Solder-less breadboard, and jumper wire kit
2 – AD8561 Comparators
1 – 2N3904 NPN transistor
2 – 1N914 small signal diodes
1 – LED ( any color )
3 – 10KΩ resistor
1 – 20KΩ resistor
1 – 470Ω resistor

university/courses/electronics/electronics-lab-window-comp-tmp01.1520351308.txt.gz · Last modified: 06 Mar 2018 16:48 by Antoniu Miclaus