Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (06 Mar 2018 14:32) was approved by Antoniu Miclaus.

This is an old revision of the document!


Activity: Temperature Control using Window Comparator

Objective

The objective of this lab activity is to use two high speed voltage comparators as a Window-Comparator and program the TMP01 Low Power Programmable Temperature Controller using this approach.

A Window-Comparator is a circuit configuration, usually consisting of a pair of voltage comparators (inverting and non-inverting), in which the output indicates whether an input signal is within the voltage range bounded by two different thresholds. One which triggers an op-amp comparator on detection of some upper voltage threshold, VREF(UPPER) and one which triggers an op-amp comparator on detection of a lower voltage threshold level, VREF(LOWER). The voltage levels between these two upper and lower reference voltages is called the “window”

university/courses/electronics/electronics-lab-window-comp-tmp01.1520343095.txt.gz · Last modified: 06 Mar 2018 14:31 by Antoniu Miclaus