This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-window-comp-tmp01 [06 Mar 2018 16:48] – add materials Antoniu Miclaus | university:courses:electronics:electronics-lab-window-comp-tmp01 [23 Aug 2019 14:14] – Antoniu Miclaus | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Objective ===== | ===== Objective ===== | ||
- | The objective of this lab activity is to use two high speed voltage comparators as a Window-Comparator and program the [[http:// | + | The objective of this lab activity is to use two high speed voltage comparators as a Window-Comparator and program the TMP01 Low Power Programmable Temperature Controller using this approach. |
A Window-Comparator is a circuit configuration, | A Window-Comparator is a circuit configuration, | ||
Line 11: | Line 11: | ||
ADALM2000 Active Learning Module\\ | ADALM2000 Active Learning Module\\ | ||
Solder-less breadboard, and jumper wire kit\\ | Solder-less breadboard, and jumper wire kit\\ | ||
- | 2 – AD8561 Comparators | + | 2 – AD8561 Comparators\\ |
- | 1 – 2N3904 NPN transistor | + | 1 – 2N3904 NPN transistor\\ |
- | 2 – 1N914 small signal diodes | + | 2 – 1N914 small signal diodes\\ |
- | 1 – LED ( any color ) | + | 1 – LED ( any color )\\ |
- | 3 – 10KΩ resistor | + | 3 – 10KΩ resistor\\ |
- | 1 – 20KΩ resistor | + | 1 – 20KΩ resistor\\ |
- | 1 – 470Ω resistor | + | 1 – 470Ω resistor\\ |
+ | |||
+ | ===== Window Comparator ===== | ||
+ | |||
+ | ==== Background ==== | ||
+ | |||
+ | Consider the circuit presented in Figure 1. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The circuit uses a voltage divider network, formed of three equal value resistors R1 = R2 = R3. The voltage drops across each resistor will also be equal at one-third of the reference voltage (V< | ||
+ | |||
+ | Considering that we use the When V< | ||
+ | |||
+ | When V< | ||
+ | |||
+ | When V< | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | |||
+ | Build the following breadboard circuit for the window comparator circuit. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Procedure ==== | ||
+ | |||
+ | Use the first waveform generator (W1) as source to provide a Triangular signal with 5V amplitude peak-to-peak, | ||
+ | |||
+ | Use the second waveform generator (W2) as 5V constant reference voltage. | ||
+ | |||
+ | Supply the circuit using the 5V power supply. | ||
+ | |||
+ | Configure the scope so that output signal is displayed on channel 2 and the input signal is displayed on channel 1. | ||
+ | |||
+ | A plot example is presented in Figure 3. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | On the plot the " | ||
+ | |||
+ | ===== Temperature Control ===== | ||
+ | |||
+ | ==== Background ==== | ||
+ | |||
+ | An example of a window comparator application is a simple temperature controller circuit (Figure 2). The temperature sensor, TMP01, has the dual comparator configuration of figure 1 built in. By choosing the proper values for R< | ||
+ | |||
+ | The TMP01 is a linear voltage-output temperature sensor, with a window comparator that can be programmed by the user to activate one of two open-collector outputs when a predetermined temperature set point voltage has been exceeded. A low drift voltage reference is available for set point programming. By connecting the two open collector outputs together as a single wire OR output we can obtain a signal which is at a logic high when the ambient temperature is within the target window. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Programming TMP01 ==== | ||
+ | |||
+ | In the basic fixed set point application utilizing a simple resistor ladder voltage divider, the desired temperature set points are programmed in the following sequence: | ||
+ | |||
+ | 1. Select the desired hysteresis temperature. | ||
+ | |||
+ | 2. Calculate the hysteresis current I< | ||
+ | |||
+ | 3. Select the desired set point temperatures. | ||
+ | |||
+ | 4. Calculate the individual resistor divider ladder values needed to develop the desired comparator set point voltages at SET HIGH and SET LOW. | ||
+ | |||
+ | The hysteresis current is readily calculated. For example, for 2 degrees of hysteresis, I< | ||
+ | |||
+ | V< | ||
+ | |||
+ | V< | ||
+ | |||
+ | R< | ||
+ | |||
+ | R< | ||
+ | |||
+ | R< | ||
+ | |||
+ | The total R< | ||
+ | |||
+ | I< | ||
+ | |||
+ | Since VREF = 2.5 V, with a reference load resistance of 357 kΩ or greater (output current 7 μA or less), the temperature setpoint hysteresis is zero degrees. Larger values of load resistance only decrease the output current below 7 μA and have no effect on the operation of the device. The amount of hysteresis is determined by selecting a value of load resistance for VREF. | ||
+ | |||
+ | ==== Tasks ==== | ||
+ | |||
+ | 1. Build the following circuit: | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | Measure VPTAT output value and compute the actual measured temperature in degrees Kelvin and degrees Celsius. | ||
+ | |||
+ | 2. Build the following circuit: | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | 2.a. Identify the components and try to draw the circuit schematic. | ||
+ | |||
+ | 2.b. Using the information provided by the breadboard circuit, compute the following parameters: | ||
+ | |||
+ | * I< | ||
+ | * V< | ||
+ | * V< | ||
+ | * T< | ||
+ | * T< | ||
+ | |||
+ | 2.c. How many degrees is the temperature setpoint hysteresis? How can you change this value? | ||
+ | |||
+ | 2.d. How does the circuit work? When will LED1 (red) and LED2 (blue) turn on? Explain your answer. | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Lab Resources: | ||
+ | * Fritzing files: [[ https:// | ||
+ | * LTspice files: [[ https:// | ||
+ | </ | ||
+ | ===== Further Reading ===== | ||
+ | |||
+ | Additional resources: | ||
+ | |||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | **Return to Lab Activity [[university: | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||