university:courses:electronics:electronics-lab-window-comp-tmp01 [09 Mar 2018 14:12]
Antoniu Miclaus add task 2 + further reading
university:courses:electronics:electronics-lab-window-comp-tmp01 [03 Jan 2021 22:21] (current)
Robin Getz fix links
Line 47: Line 47:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator (W1) as source to provide a Triangular signal with 5V amplitude, 100Hz frequency and 2.5V offset.+Use the first waveform generator (W1) as source to provide a Triangular signal with 5V amplitude ​peak-to-peak, 100Hz frequency and 2.5V offset.
  
 Use the second waveform generator (W2) as 5V constant reference voltage. Use the second waveform generator (W2) as 5V constant reference voltage.
Line 123: Line 123:
 2.a. Identify the components and try to draw the circuit schematic. 2.a. Identify the components and try to draw the circuit schematic.
  
-2.b. Using the information provided ​in the breadboard circuit, compute the following parameters:+2.b. Using the information provided ​by the breadboard circuit, compute the following parameters:
  
   * I<​sub>​VREF</​sub>​   * I<​sub>​VREF</​sub>​
Line 131: Line 131:
   * T<​sub>​SETLOW</​sub>​   * T<​sub>​SETLOW</​sub>​
  
-2.c. How many degrees is the temperature setpoint hysteresis?+2.c. How many degrees is the temperature setpoint hysteresis? How can you change this value?
  
 2.d. How does the circuit work? When will LED1 (red) and LED2 (blue) turn on? Explain your answer. 2.d. How does the circuit work? When will LED1 (red) and LED2 (blue) turn on? Explain your answer.
  
 +<WRAP round download>​
 +**Lab Resources:​**
 +  * Fritzing files: [[downgit>​education_tools/​tree/​master/​m2k/​fritzing/​temp_ctrl_bb | temp_ctrl_bb]]
 +  * LTspice files: [[downgit>​education_tools/​tree/​master/​m2k/​fritzing/​temp_ctrl_ltspice | temp_ctrl_ltspice]]
 +</​WRAP>​
 ===== Further Reading ===== ===== Further Reading =====
  
 Additional resources: Additional resources:
  
-  * [[http://​www.analog.com/​static/​imported-files/​data_sheets/​TMP01.pdf|TMP01 Low Power Programmable Temperature Controller]] +  * [[adi>static/​imported-files/​data_sheets/​TMP01.pdf|TMP01 Low Power Programmable Temperature Controller]] 
-  * [[http://​www.analog.com/​library/​analogdialogue/​archives/​42-10/​testing_comparators.html|Adding Test Capability to a Window Comparator]]+  * [[adi>library/​analogdialogue/​archives/​42-10/​testing_comparators.html|Adding Test Capability to a Window Comparator]]
  
 **Return to Lab Activity [[university:​courses:​electronics:​labs|Table of Contents]]** **Return to Lab Activity [[university:​courses:​electronics:​labs|Table of Contents]]**
university/courses/electronics/electronics-lab-window-comp-tmp01.txt · Last modified: 03 Jan 2021 22:21 by Robin Getz