university:courses:electronics:electronics-lab-variable-gain-amplifier [15 Jul 2019 17:03]
Antoniu Miclaus
university:courses:electronics:electronics-lab-variable-gain-amplifier [03 Jan 2021 22:21] (current)
Robin Getz fix links
Line 42: Line 42:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. Use the second waveform generator for controlling the transistor, providing a 2V amplitude, 1Hz square wave excitation. Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.+Use the first waveform generator as source Vin to provide a 2V amplitude ​peak-to-peak, 1 kHz sine wave excitation to the circuit. Use the second waveform generator for controlling the transistor, providing a 2V amplitude, 1Hz square wave excitation. Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
  
 An animated plot is presented in Figure 3. An animated plot is presented in Figure 3.
Line 74: Line 74:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. ​ Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.+Use the first waveform generator as source Vin to provide a 2V amplitude ​peak-to-peak, 1 kHz sine wave excitation to the circuit. ​ Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
  
 By varying the value of the potentiometer,​ an animated plot is presented in Figure 6. By varying the value of the potentiometer,​ an animated plot is presented in Figure 6.
Line 106: Line 106:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. ​ Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.+Use the first waveform generator as source Vin to provide a 2V amplitude ​peak-to-peak, 1 kHz sine wave excitation to the circuit. ​ Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
  
 By varying the value of the potentiometer,​ an animated plot is presented in Figure 9. By varying the value of the potentiometer,​ an animated plot is presented in Figure 9.
Line 128: Line 128:
 <WRAP round download>​ <WRAP round download>​
 **Lab Resources:​** **Lab Resources:​**
-  * Fritzing files: [[ https://​minhaskamal.github.io/​DownGit/#/​home?​url=https://​github.com/​analogdevicesinc/​education_tools/​tree/​master/​m2k/​fritzing/​var_gain_amp_bb | var_gain_amp_bb]] +  * Fritzing files: [[downgit>education_tools/​tree/​master/​m2k/​fritzing/​var_gain_amp_bb | var_gain_amp_bb]] 
-  * LTspice files: [[ https://​minhaskamal.github.io/​DownGit/#/​home?​url=https://​github.com/​analogdevicesinc/​education_tools/​tree/​master/​m2k/​ltspice/​var_gain_amp_ltspice | var_gain_amp_ltspice]]+  * LTspice files: [[downgit>education_tools/​tree/​master/​m2k/​ltspice/​var_gain_amp_ltspice | var_gain_amp_ltspice]]
 </​WRAP>​ </​WRAP>​
  
 Some additional resources: Some additional resources:
-  * [[http://​www.analog.com/​en/​analog-dialogue/​articles/​x-amp-45-db-500-mhz-variable-gain-amplifier.html|X-Amp™,​ A New 45-dB, 500-MHz Variable-Gain Amplifier (VGA) Simplifies Adaptive Receiver Designs]] +  * [[adi>en/​analog-dialogue/​articles/​x-amp-45-db-500-mhz-variable-gain-amplifier.html|X-Amp™,​ A New 45-dB, 500-MHz Variable-Gain Amplifier (VGA) Simplifies Adaptive Receiver Designs]] 
-  * [[http://​www.analog.com/​en/​analog-dialogue/​articles/​reinvent-the-signal-generator.html|Two New Devices Help Reinvent the Signal Generator]]+  * [[adi>en/​analog-dialogue/​articles/​reinvent-the-signal-generator.html|Two New Devices Help Reinvent the Signal Generator]]
  
 **Return to Lab Activity [[university:​courses:​electronics:​labs|Table of Contents]]** **Return to Lab Activity [[university:​courses:​electronics:​labs|Table of Contents]]**
university/courses/electronics/electronics-lab-variable-gain-amplifier.1563203035.txt.gz · Last modified: 15 Jul 2019 17:03 by Antoniu Miclaus