This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-variable-gain-amplifier [26 Mar 2018 13:48] – add Questions and Further Reading Antoniu Miclaus | university:courses:electronics:electronics-lab-variable-gain-amplifier [23 Aug 2019 15:14] – Antoniu Miclaus | ||
---|---|---|---|
Line 26: | Line 26: | ||
Consider the circuit schematic presented in Figure 1. | Consider the circuit schematic presented in Figure 1. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 42: | Line 42: | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. Use the second waveform generator for controlling the transistor, providing a 2V amplitude, 1Hz square wave excitation. Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2. | + | Use the first waveform generator as source Vin to provide a 2V amplitude |
An animated plot is presented in Figure 3. | An animated plot is presented in Figure 3. | ||
Line 58: | Line 58: | ||
Consider the circuit schematic presented in Figure 4. | Consider the circuit schematic presented in Figure 4. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 74: | Line 74: | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. | + | Use the first waveform generator as source Vin to provide a 2V amplitude |
By varying the value of the potentiometer, | By varying the value of the potentiometer, | ||
Line 90: | Line 90: | ||
Consider the circuit schematic presented in Figure 7. | Consider the circuit schematic presented in Figure 7. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 106: | Line 106: | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. | + | Use the first waveform generator as source Vin to provide a 2V amplitude |
By varying the value of the potentiometer, | By varying the value of the potentiometer, | ||
Line 125: | Line 125: | ||
===== Further Reading ===== | ===== Further Reading ===== | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Lab Resources: | ||
+ | * Fritzing files: [[ https:// | ||
+ | * LTspice files: [[ https:// | ||
+ | </ | ||
Some additional resources: | Some additional resources: |