This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-variable-gain-amplifier [15 Jul 2019 17:03] – Antoniu Miclaus | university:courses:electronics:electronics-lab-variable-gain-amplifier [23 Aug 2019 15:14] – Antoniu Miclaus | ||
---|---|---|---|
Line 42: | Line 42: | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. Use the second waveform generator for controlling the transistor, providing a 2V amplitude, 1Hz square wave excitation. Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2. | + | Use the first waveform generator as source Vin to provide a 2V amplitude |
An animated plot is presented in Figure 3. | An animated plot is presented in Figure 3. | ||
Line 74: | Line 74: | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. | + | Use the first waveform generator as source Vin to provide a 2V amplitude |
By varying the value of the potentiometer, | By varying the value of the potentiometer, | ||
Line 106: | Line 106: | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. | + | Use the first waveform generator as source Vin to provide a 2V amplitude |
By varying the value of the potentiometer, | By varying the value of the potentiometer, |