Last revision Both sides next revision
university:courses:electronics:electronics-lab-variable-gain-amplifier [26 Mar 2018 13:30]
Antoniu Miclaus add Variable Gain Inverting/Non-Inverting Amplifier using potetiometer
university:courses:electronics:electronics-lab-variable-gain-amplifier [25 Jun 2020 22:07]
external edit
Line 26: Line 26:
 Consider the circuit schematic presented in Figure 1. Consider the circuit schematic presented in Figure 1.
  
-<WRAP centeralign>​ {{:​university:​courses:​electronics:​var_gain_amp_crl-sch.png|}} </​WRAP>​+<WRAP centeralign>​ {{ :​university:​courses:​electronics:​vctrl_amp_transistor.png|}} </​WRAP>​
  
 <WRAP centeralign>​ Figure 1. Voltage control using transistor </​WRAP>​ <WRAP centeralign>​ Figure 1. Voltage control using transistor </​WRAP>​
Line 42: Line 42:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. Use the second waveform generator for controlling the transistor, providing a 2V amplitude, 1Hz square wave excitation. Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.+Use the first waveform generator as source Vin to provide a 2V amplitude ​peak-to-peak, 1 kHz sine wave excitation to the circuit. Use the second waveform generator for controlling the transistor, providing a 2V amplitude, 1Hz square wave excitation. Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
  
 An animated plot is presented in Figure 3. An animated plot is presented in Figure 3.
Line 58: Line 58:
 Consider the circuit schematic presented in Figure 4. Consider the circuit schematic presented in Figure 4.
  
-<WRAP centeralign>​ {{:​university:​courses:​electronics:​var_gain_amp_pot2-sch.png?500|}} </​WRAP>​+<WRAP centeralign>​ {{ :​university:​courses:​electronics:​var_g_invert_amp_pot.png|}} </​WRAP>​
  
 <WRAP centeralign>​ Figure 4. Variable Gain Inverting Amplifier using potetiometer </​WRAP>​ <WRAP centeralign>​ Figure 4. Variable Gain Inverting Amplifier using potetiometer </​WRAP>​
Line 74: Line 74:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. ​ Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.+Use the first waveform generator as source Vin to provide a 2V amplitude ​peak-to-peak, 1 kHz sine wave excitation to the circuit. ​ Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
  
 By varying the value of the potentiometer,​ an animated plot is presented in Figure 6. By varying the value of the potentiometer,​ an animated plot is presented in Figure 6.
Line 90: Line 90:
 Consider the circuit schematic presented in Figure 7. Consider the circuit schematic presented in Figure 7.
  
-<WRAP centeralign>​ {{:​university:​courses:​electronics:​var_gain_amp_pot-sch.png?500|}} </​WRAP>​+<WRAP centeralign>​ {{ :​university:​courses:​electronics:​var_gain_inv_noninv.png|}} </​WRAP>​
  
 <WRAP centeralign>​ Figure 7. Variable Gain Inverting/​Non-Inverting Amplifier using potetiometer </​WRAP>​ <WRAP centeralign>​ Figure 7. Variable Gain Inverting/​Non-Inverting Amplifier using potetiometer </​WRAP>​
Line 106: Line 106:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. ​ Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.+Use the first waveform generator as source Vin to provide a 2V amplitude ​peak-to-peak, 1 kHz sine wave excitation to the circuit. ​ Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
  
 By varying the value of the potentiometer,​ an animated plot is presented in Figure 9. By varying the value of the potentiometer,​ an animated plot is presented in Figure 9.
Line 112: Line 112:
 <WRAP centeralign>​ {{:​university:​courses:​electronics:​var_gain_amp_pot-wav.gif|}} </​WRAP>​ <WRAP centeralign>​ {{:​university:​courses:​electronics:​var_gain_amp_pot-wav.gif|}} </​WRAP>​
  
-<WRAP centeralign>​ Figure 9. Variable Gain Inverting/​Non-Inverting Amplifier using potetiometer ​- waveforms </​WRAP>​+<WRAP centeralign>​ Figure 9. Variable Gain Inverting/​Non-Inverting Amplifier using potentiometer ​- waveforms </​WRAP>​
  
 Using this configuration,​ the output is amplified varying between +-Vin. Using this configuration,​ the output is amplified varying between +-Vin.
 +
 +===== Questions =====
 +
 +1. Which are the gain values for each of the circuits used in this lab activity?
 +
 +2. Based on the input signals and the computed gains, which are the expected output values? Compute and compare them with the measured values.
 +
 +3. Considering the circuit in Figure 7, how can you increase the output range above +-Vin?
 +
 +===== Further Reading =====
 +
 +<WRAP round download>​
 +**Lab Resources:​**
 +  * Fritzing files: [[downgit>​education_tools/​tree/​master/​m2k/​fritzing/​var_gain_amp_bb | var_gain_amp_bb]]
 +  * LTspice files: [[downgit>​education_tools/​tree/​master/​m2k/​ltspice/​var_gain_amp_ltspice | var_gain_amp_ltspice]]
 +</​WRAP>​
 +
 +Some additional resources:
 +  * [[http://​www.analog.com/​en/​analog-dialogue/​articles/​x-amp-45-db-500-mhz-variable-gain-amplifier.html|X-Amp™,​ A New 45-dB, 500-MHz Variable-Gain Amplifier (VGA) Simplifies Adaptive Receiver Designs]]
 +  * [[http://​www.analog.com/​en/​analog-dialogue/​articles/​reinvent-the-signal-generator.html|Two New Devices Help Reinvent the Signal Generator]]
 +
 +**Return to Lab Activity [[university:​courses:​electronics:​labs|Table of Contents]]**
 +
 +
  
university/courses/electronics/electronics-lab-variable-gain-amplifier.txt · Last modified: 03 Jan 2021 22:21 by Robin Getz