This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-speaker [27 Mar 2017 16:55] – [Procedure:] Doug Mercer | university:courses:electronics:electronics-lab-speaker [24 Jul 2017 16:17] – change amplitude value to peak-peak Antoniu Miclaus | ||
---|---|---|---|
Line 53: | Line 53: | ||
=====Procedure: | =====Procedure: | ||
- | Start the Scopy software. Select the Network Analyzer instrument. Set the start frequency to 10Hz and the end frequency to 1KHz. Set the amplitude to 4 Volts and the offset to 0V. Set the max gain to 1X. Under the Settings drop down tab open the options window and set the settle time to 40 and the FFT window to cosine. | + | Start the Scopy software. Select the Network Analyzer instrument. Set the start frequency to 10Hz and the end frequency to 1KHz. Set the amplitude to 8 Volts and the offset to 0V. Set the max gain to 1X. Under the Settings drop down tab open the options window and set the settle time to 40 and the FFT window to cosine. |
A few words on why these setting should be adjusted. As the frequency is swept the AWG output is stopped briefly between frequency steps and the signal driving the speaker will be turned off. The speaker is a mechanical system with resonance and this step change in the driving signal will cause it to ring at the resonate frequency. In order to make an accurate measurement at the driving frequency we must wait for the ringing to die out. The amount of time needed will depend on the particular speaker being measured. The 40 mSec suggested above was the correct value for the speaker used in this example. Your results may vary depending on your particular speaker. Switching to the cosine window function gives a more accurate amplitude result. | A few words on why these setting should be adjusted. As the frequency is swept the AWG output is stopped briefly between frequency steps and the signal driving the speaker will be turned off. The speaker is a mechanical system with resonance and this step change in the driving signal will cause it to ring at the resonate frequency. In order to make an accurate measurement at the driving frequency we must wait for the ringing to die out. The amount of time needed will depend on the particular speaker being measured. The 40 mSec suggested above was the correct value for the speaker used in this example. Your results may vary depending on your particular speaker. Switching to the cosine window function gives a more accurate amplitude result. |