Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:electronics-lab-scr [05 Mar 2019 12:34]
amiclaus [LATCH-UP]
university:courses:electronics:electronics-lab-scr [23 Aug 2019 14:01] (current)
amiclaus
Line 103: Line 103:
 =====Hardware Setup:===== =====Hardware Setup:=====
  
-AWG1 should be configured as a sine wave with an amplitude of 10 V, zero offset and a frequency of 100  +AWG1 should be configured as a sine wave with an amplitude of 10 V peak-to-peak, zero offset and a frequency of 100  
-Hz. AWG2 should be configured as a square wave with an amplitude of 800 mV, 400 mV offset, a frequency ​+Hz. AWG2 should be configured as a square wave with an amplitude of 800 mV peak-to-peak, 400 mV offset, a frequency ​
 of 100 Hz. Be sure to run the two AWG channels synchronously. of 100 Hz. Be sure to run the two AWG channels synchronously.
 {{ :​university:​courses:​electronics:​ascr_bb.png?​ |}} {{ :​university:​courses:​electronics:​ascr_bb.png?​ |}}
university/courses/electronics/electronics-lab-scr.txt · Last modified: 23 Aug 2019 14:01 by amiclaus