This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-scr [05 Mar 2019 12:34] – [LATCH-UP] Antoniu Miclaus | university:courses:electronics:electronics-lab-scr [23 Aug 2019 14:01] – Antoniu Miclaus | ||
---|---|---|---|
Line 103: | Line 103: | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | AWG1 should be configured as a sine wave with an amplitude of 10 V, zero offset and a frequency of 100 | + | AWG1 should be configured as a sine wave with an amplitude of 10 V peak-to-peak, zero offset and a frequency of 100 |
- | Hz. AWG2 should be configured as a square wave with an amplitude of 800 mV, 400 mV offset, a frequency | + | Hz. AWG2 should be configured as a square wave with an amplitude of 800 mV peak-to-peak, 400 mV offset, a frequency |
of 100 Hz. Be sure to run the two AWG channels synchronously. | of 100 Hz. Be sure to run the two AWG channels synchronously. | ||
{{ : | {{ : |