This is an old revision of the document!
In this laboratory we examine the pulse width modulation and its usage within a variety of applications.
Pulse Width Modulation (PWM) Signal is a method for generating an analog signal using a digital source. A PWM signal consists of two main components that define its behavior: a duty cycle and a frequency.
The duty cycle describes the amount of time the signal is in a high (on) state as a percentage of the total time of it takes to complete one cycle.
The following diagram shows pulse trains at 0%, 25%, and 100% duty cycle.
The frequency determines how fast the PWM completes a cycle, and therefore how fast it switches between high and low states.
By varying a digital signal off and on at a fast enough rate, and with a certain duty cycle, the output will appear to behave like a constant voltage analog signal when providing power to devices.
The PWM is a technique used in transmission of information by encoding a message into a pulsing signal, also for power control of electronic devices such as motors and as principal algorithm for photo-voltaic solar battery chargers.
ADALM2000 Active Learning Module
Solder-less breadboard, and jumper wire kit
1 OP97 operational amplifier
1 1kΩ resistor
1 10kΩ potentiometer
Pulse Width Modulation (PWM) is a technique to generate low frequency output signals from high frequency pulses. Rapidly switching the output voltage of an inverter leg between the upper and lower DC rail voltages, the low frequency output can be though of as the average of voltage over a switching period.
In its simplest form PWM output signals are constructed by comparing two control signals, a carrier signal and a modulation signal. This is known as carrier-based PWM. The carrier signal is a high frequency (switching frequency) triangular waveform. The modulation signal can be any shape.
Using this approach, the output waveform can be made to follow any desired waveform shape. With machines, sinusoidal and trapezoidal waveform shapes are among the most common.
Consider the circuit in Figure 1.
Figure 1. PWM Principle
Following the description of the PWM principle, we use the negative input of the operational amplifier for carrier, while the positive input for the modulation signal.
Build the following breadboard circuit for Pulse Width Modulation.
Figure 2. PWM Principle breadboard circuit
Use the first waveform generator as carrier signal providing a 4V amplitude, 2.5V offset, 1 kHz triangle wave excitation to the circuit. Use the second waveform generator as modulation signal with 3V amplitude, 2.5V offset, 50Hz sine wave.
In the figure there are presented the two signal generator channels containing the two input signals (orange - carrier signal, purple - modulation signal).
Figure 3. Input Signals
Supply the op amp to +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
A plot with the output signal on channel 2 of the scope is presented in Figure 4.
Figure 4. PWM output
If the peak of the modulation is less than the peak of the carrier signal, the output will follow the shape of the modulation signal. If instantaneous magnitude of the modulation signal is greater than the carried signal at a point in time, the output voltage should be connected to positive side of the supply (high state). If the carrier signal is greater than the modulation signal, the output should be connected to the negative side of the supply (low state).
For this particular application we will use a simple operational amplifier in a switching mode configuration (see Activity: Op Amp as Comparator for further details) in order to emphasize the pulse width control of the output signal.
Consider the circuit in Figure 5.
Figure 5. Pulse Width Control using Reference Voltage
The circuit works as a simple comparator where the negative input of the operational amplifier is connected to the input waveform, while the positive input acts as a threshold voltage which establishes when the transitions between high voltage output and low voltage output occur. The potentiometer acts as a voltage divider for the input reference voltage, adjusting the threshold voltage, and implicitly the duty cycle of the output signal.
Build the following breadboard circuit for Pulse Width Control using Reference Voltage.
Figure 6. Pulse Width Control using Reference Voltage - Breadboard circuit
Use the first waveform generator as source Vin to provide a 5V amplitude, 1 kHz triangle wave excitation to the circuit. Use the second waveform generator as constant voltage source with 5V amplitude. Supply the op amp to +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
An animated plot is presented in Figure 7.
Figure 7. Pulse Width Control using Reference Voltage - waveforms
The output signal is a squared shaped determined by the two possible output values. We can notice that, by varying the potentiometer value, the duty cycle of the signal changes, while the frequency remains constant.