This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-pulse-width-modulation [15 Jul 2019 11:42] – Circuit schematics have been replaced Pop Andreea | university:courses:electronics:electronics-lab-pulse-width-modulation [27 Jan 2021 22:36] (current) – use wp> interwiki links Robin Getz | ||
---|---|---|---|
Line 57: | Line 57: | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as the carrier signal providing a 4V amplitude, 2.5V offset, 1 kHz triangle wave excitation to the circuit. Use the second waveform generator as the modulation signal with 3V amplitude, 2.5V offset, 50Hz sine wave. | + | Use the first waveform generator as the carrier signal providing a 4V amplitude |
Supply the op amp with +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2 . | Supply the op amp with +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2 . | ||
Line 103: | Line 103: | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as source Vin to provide a 5V amplitude, 1 kHz triangle wave excitation to the circuit. Use the second waveform generator as constant voltage source with 5V amplitude. | + | Use the first waveform generator as source Vin to provide a 5V amplitude |
Supply the op amp to +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2. | Supply the op amp to +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2. | ||
Line 189: | Line 189: | ||
<WRAP round download> | <WRAP round download> | ||
**Lab Resources: | **Lab Resources: | ||
- | * Fritzing files: [[ https:// | + | * Fritzing files: [[downgit>education_tools/ |
- | * LTspice files: [[ https:// | + | * LTspice files: [[downgit>education_tools/ |
</ | </ | ||
===== Further Reading ===== | ===== Further Reading ===== | ||
Some additional resources: | Some additional resources: | ||
- | * [[https:// | + | * [[wp>Pulse-width_modulation|Pulse-width modulation]] |
* [[university: | * [[university: | ||
- | * [[http:// | + | * [[adi>en/ |
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||