Wiki

The most recent version of this page is a draft.DiffThis version is outdated by a newer approved version.DiffThis version (14 Dec 2018 11:38) was approved by Antoniu Miclaus.The Previously approved version (24 Aug 2017 13:33) is available.Diff

This is an old revision of the document!


Activity: LED as light sensor

Objective:

The objective of this Lab activity is to explore the use of LEDs as a photodiode light sensor and the use of NPN and Darlington connected NPN transistors as interface circuits for the light sensor.

Background:

When exposed to light photodiodes produce a current that is directly proportional to the intensity of the light. This light generated current flows in the opposite direction to current in a normal diode or LED. As more photons hit the photodiode the current increases causing a voltage across the diode. As the voltage across the diode increases the linearity decreases.

In addition to emitting light, an LED can be used as a photodiode light sensor / detector. This capability may be used in a variety of applications including ambient light level sensor and bidirectional communications. As a photodiode, an LED is sensitive to wavelengths equal to or shorter than the predominant wavelength it emits. A green LED would be sensitive to blue light and to some green light, but not to yellow or red light. For example, a red LED will detect light emitted by a yellow LED and a yellow LED will detect light emitted by a green LED but a green LED will not detect light emitted by a red or yellow LED. All three LEDs will detect “white” light or light from a blue LED. White light contains a blue light component which can be detected by the green LED. Recall that visible light wavelengths can be listed from longest wavelength to shortest wavelength as Red, Orange, Yellow, Green, Blue, Indigo, Violet (remember the mnemonic “Roy G. Biv”). Violet is the shortest wavelength light with the most energetic photons and red has the longest wavelength light with the least energetic photons of all of the visible colors of light. LED's with clear plastic encapsulation will be more sensitive to broad-spectrum illumination (like general room lighting) than LED's with colored encapsulation (such as those included in the ADALP2000 Analog Parts Kit).

To use the LED as an optical detector, do not forward bias the LED into quadrant #1 of the current-voltage (I-V) curve. (Quadrant 1 is when the operating voltage and current are both positive.) Allow the LED to operate in the solar cell mode, quadrant #4 (operating voltage is positive, current is negative), or in the photodiode mode quadrant #3 (operating voltage is negative, current is negative). In the solar cell mode, no applied bias voltage is used. The solar cell (or LED in this case) generates its own current and voltage.

Materials:

ADALM2000 Active Learning Module
Solder-less breadboard
Jumper wires
2 - 2N3904 NPN transistors ( or SSM2212 NPN matched pair )
1 - 100KΩ resistor
1 - 2.2KΩ resistor
3 - LEDs ( multiple red, yellow and green colors )
1 - Infrared LED ( QED-123 )

Directions:

On your solder-less breadboard construct the LED light sensor circuit as shown in figure 1. Notice that the LED diode, D1, is reverse biased i.e. opposite to how it would be connected as a light emitter. The photo generated current will flow into Q1 as base current and will appear in the collector multiplied by the current gain, ß of the transistor.

Figure 1 LED and single common emitter NPN light sensor

Hardware Setup:

Figure 2 LED and single common emitter NPN light sensor Breadboard Circuit

Use the variable positive power supply from the ADALM2000 module set to +5 V to power your circuit. Use scope channel 1 to monitor the voltage at the collector node of Q1.

Procedure:

Insert a red, yellow or green LED into the circuit as shown one at a time. Try exposing the three different color LEDs from your ADALP2000 Analog Parts Kit to different light sources such as standard incandescent, florescent and LED lights held at differing distances from the LED sensor. Observe the voltage waveform seen at the collector of Q1. Try inserting the infrared LED from your kit and observing how it responds to the light from the different sources. Try increasing the sensitivity or gain by increasing the value of RL to 200KΩ or 470KΩ.

Figure 3 Red LED and single common emitter NPN light sensor - Led light max distance

Figure 4 Red LED and single common emitter NPN light sensor - Led light medium distance

Figure 5 Red LED and single common emitter NPN light sensor - Led light min distance

Step 2 Directions:

Change the circuit on your breadboard to the Darlington configuration shown in figure 6. Be sure to turn off the power supply before making any changes to the circuit. With the Darlington connected transistors the emitter current of Q2 becomes the base current of Q1 such that the photo generated current from the LED D1 is now multiplied by ß2 and will appear in the load resistor RL from the collectors of Q1 and Q2. Because of this much higher current gain we can use a much lower value load resistor.

Figure 6 LED and Darlington connected NPN light sensor

Step 2 Hardware Setup:

Figure 7 LED and Darlington connected light sensor Breadboard Circuit

Step 2 Procedure:

Repeat the same procedure of inserting the various LEDs into the circuit for D1 and measuring the response to the various light sources and record them in your lab report.

Figure 8 Red LED and Darlington connected light sensor - Led light max distance

Figure 9 Red LED and Darlington connected light sensor - Led light medium distance

Figure 10 Red LED and Darlington connected light sensor - Led light min distance

Questions:

How well does the red LED respond to the various light sources? Does it respond to another red or yellow or green LED used as a light emitter? How about the yellow and green LEDs? Is the infrared LED sensitive to the same or different wavelengths of light compared to the visible light LEDs? Which is the most sensitive to standard household lights such as incandescent and compact florescent bulbs?

How does the sensitivity of the Darlington connected configuration compare to the single common emitter configuration? Are the minimum and maximum voltages the same for both configurations? If not, why?

Resources:

For Further Reading:

https://en.wikipedia.org/wiki/LED
https://en.wikipedia.org/wiki/LED_circuit
https://en.wikipedia.org/wiki/Photodiode

Return to Lab Activity Table of Contents.

university/courses/electronics/electronics-lab-led-sensor.1544783918.txt.gz · Last modified: 14 Dec 2018 11:38 by Antoniu Miclaus