This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-lco [24 Jul 2017 16:08] – change amplitude value to peak-peak Antoniu Miclaus | university:courses:electronics:electronics-lab-lco [13 Jun 2022 20:07] (current) – [Background:] Doug Mercer | ||
---|---|---|---|
Line 25: | Line 25: | ||
Below in figure 2 is the schematic and pinout for the CD4007: | Below in figure 2 is the schematic and pinout for the CD4007: | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 47: | Line 47: | ||
==== Hardware Setup: ==== | ==== Hardware Setup: ==== | ||
- | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. | + | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude |
==== Procedure: ==== | ==== Procedure: ==== |