Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revisionBoth sides next revision
university:courses:electronics:electronics-lab-lco [24 Apr 2017 08:41] – [Additional Activity:] rename Antoniu Miclausuniversity:courses:electronics:electronics-lab-lco [24 Jul 2017 16:08] – change amplitude value to peak-peak Antoniu Miclaus
Line 47: Line 47:
 ==== Hardware Setup: ==== ==== Hardware Setup: ====
  
-Configure the waveform generator for a 1 KHz triangle wave with 2.5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div.+Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div.
  
 ==== Procedure: ==== ==== Procedure: ====
university/courses/electronics/electronics-lab-lco.txt · Last modified: 13 Jun 2022 20:07 by Doug Mercer