Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Last revision Both sides next revision
university:courses:electronics:electronics-lab-lco [24 Apr 2017 08:41]
Antoniu Miclaus [Additional Activity:] rename
university:courses:electronics:electronics-lab-lco [24 Jul 2017 16:08]
Antoniu Miclaus change amplitude value to peak-peak
Line 47: Line 47:
 ==== Hardware Setup: ==== ==== Hardware Setup: ====
  
-Configure the waveform generator for a 1 KHz triangle wave with 2.5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div.+Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div.
  
 ==== Procedure: ==== ==== Procedure: ====
university/courses/electronics/electronics-lab-lco.txt · Last modified: 23 Aug 2019 13:59 by Antoniu Miclaus