Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
university:courses:electronics:electronics-lab-lco [23 Mar 2017 16:36]
dmercer [Directions:]
university:courses:electronics:electronics-lab-lco [24 Jul 2017 16:08]
amiclaus change amplitude value to peak-peak
Line 47: Line 47:
 ==== Hardware Setup: ==== ==== Hardware Setup: ====
  
-Configure the waveform generator for a 1 KHz triangle wave with 2.5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div.+Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div.
  
 ==== Procedure: ==== ==== Procedure: ====
Line 96: Line 96:
 ==== Additional Activity: ==== ==== Additional Activity: ====
  
-Could you modify this circuit to make the frequency of the oscillator temperature dependent by substituting the photo resistor with the thermistor from the Analog Parts Kit?+Could you modify this circuit to make the frequency of the oscillator temperature dependent by substituting the photo resistor with the thermistor from the ADALP2000 ​Analog Parts Kit?
  
 **Return to Lab Activity [[university:​courses:​electronics:​labs|Table of Contents]]** **Return to Lab Activity [[university:​courses:​electronics:​labs|Table of Contents]]**
university/courses/electronics/electronics-lab-lco.txt · Last modified: 24 Jul 2017 16:08 by amiclaus