This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-heartbeat [05 Mar 2019 10:47] – Antoniu Miclaus | university:courses:electronics:electronics-lab-heartbeat [30 Jan 2023 09:19] (current) – [Preamplifier] Antoniu Miclaus | ||
---|---|---|---|
Line 39: | Line 39: | ||
=====Directions===== | =====Directions===== | ||
- | On your solder-less breadboard construct the heartbeat measurement circuit (designed in ADIsim) as shown in Figure 1. | + | On your solder-less breadboard construct the heartbeat measurement circuit (designed in LTspice) as shown in Figure 1. |
- | {{: | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
- | Since the real circuit | + | The LTspice simulation uses OP284s, included in the standard set of LTspice models. The actual |
====IR LED==== | ====IR LED==== | ||
Line 92: | Line 92: | ||
=====Simulation===== | =====Simulation===== | ||
- | Considering the circuit designed in ADIsim, two types of simulation are made: | + | Considering the circuit designed in LTspice, two types of simulation are made: |
*Transient - Connect at the input of the circuit a waveform generation source. Configure the source to generate a sine with amplitude of 500uV, frequency 2Hz and 500mV offset. Observe the output signal amplitude in order to determine graphically the total gain of the circuit(Figure 2). | *Transient - Connect at the input of the circuit a waveform generation source. Configure the source to generate a sine with amplitude of 500uV, frequency 2Hz and 500mV offset. Observe the output signal amplitude in order to determine graphically the total gain of the circuit(Figure 2). | ||
Line 147: | Line 147: | ||
<WRAP round download> | <WRAP round download> | ||
** Lab Resources: | ** Lab Resources: | ||
- | * LTSpice files: [[ https:// | + | * LTSpice files: [[downgit>education_tools/ |
- | * ADIsimPE files: [[ https:// | + | * Fritzing files: [[downgit>education_tools/ |
- | * Fritzing files: [[ https:// | + | |
</ | </ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: |