This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-heartbeat [15 Jul 2019 16:28] – Circuit schematic replaced Pop Andreea | university:courses:electronics:electronics-lab-heartbeat [23 Aug 2019 15:09] – Antoniu Miclaus | ||
---|---|---|---|
Line 39: | Line 39: | ||
=====Directions===== | =====Directions===== | ||
- | On your solder-less breadboard construct the heartbeat measurement circuit (designed in ADIsim) as shown in Figure 1. | + | On your solder-less breadboard construct the heartbeat measurement circuit (designed in LTspice) as shown in Figure 1. |
{{ : | {{ : | ||
Line 92: | Line 92: | ||
=====Simulation===== | =====Simulation===== | ||
- | Considering the circuit designed in ADIsim, two types of simulation are made: | + | Considering the circuit designed in LTspice, two types of simulation are made: |
*Transient - Connect at the input of the circuit a waveform generation source. Configure the source to generate a sine with amplitude of 500uV, frequency 2Hz and 500mV offset. Observe the output signal amplitude in order to determine graphically the total gain of the circuit(Figure 2). | *Transient - Connect at the input of the circuit a waveform generation source. Configure the source to generate a sine with amplitude of 500uV, frequency 2Hz and 500mV offset. Observe the output signal amplitude in order to determine graphically the total gain of the circuit(Figure 2). | ||