Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
university:courses:electronics:electronics-lab-external-trigger [14 Dec 2018 11:50] – add Fritzing files Antoniu Miclaus | university:courses:electronics:electronics-lab-external-trigger [05 Mar 2019 12:45] – [Appendix: Making an inverter with the CD4007 transistor array] Antoniu Miclaus |
---|
The second Inverter is made by connecting pin 2 to V<sub>DD</sub>, pin 4 to V<sub>SS</sub>, pins 1 and 5 are connected together as the output and with pin 3 as the input. The third inverter is made by connecting pin 11 to V<sub>DD</sub>, pin 9 to V<sub>SS</sub>, pin 12 is the output and pin 10 is the input. | The second Inverter is made by connecting pin 2 to V<sub>DD</sub>, pin 4 to V<sub>SS</sub>, pins 1 and 5 are connected together as the output and with pin 3 as the input. The third inverter is made by connecting pin 11 to V<sub>DD</sub>, pin 9 to V<sub>SS</sub>, pin 12 is the output and pin 10 is the input. |
| |
| <WRAP round download> |
**Resources:** | **Resources:** |
* Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/adjust_ext_trigger_bb | adjust_ext_trigger_bb]] | * Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/adjust_ext_trigger_bb | adjust_ext_trigger_bb]] |
| </WRAP> |
| |