This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-envelope-detector [02 Mar 2018 14:45] – add frequency analysis conclusion Antoniu Miclaus | university:courses:electronics:electronics-lab-envelope-detector [10 Mar 2021 17:35] (current) – updated math equation to work with Scopy's (v1.2.0) signal generator Cristina Suteu | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Objective ===== | ===== Objective ===== | ||
- | In this lab activity we will use [[http:// | + | In this lab activity we will use [[adi>en/ |
Amplitude modulation (AM) is a modulation technique used in electronic communication, | Amplitude modulation (AM) is a modulation technique used in electronic communication, | ||
Line 41: | Line 41: | ||
Consider the circuit presented in Figure 1. | Consider the circuit presented in Figure 1. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 48: | Line 48: | ||
The capacitor in the circuit stores up charge on the rising edge, and releases it slowly through the resistor when the signal falls. The diode in series rectifies the incoming signal, allowing current flow only when the positive input terminal is at a higher potential than the negative input terminal. | The capacitor in the circuit stores up charge on the rising edge, and releases it slowly through the resistor when the signal falls. The diode in series rectifies the incoming signal, allowing current flow only when the positive input terminal is at a higher potential than the negative input terminal. | ||
- | ==== Hardware Setup: ==== | + | ==== Hardware Setup ==== |
Build the following breadboard circuit for the envelope detector circuit. | Build the following breadboard circuit for the envelope detector circuit. | ||
Line 63: | Line 63: | ||
* ω< | * ω< | ||
* A = 3 | * A = 3 | ||
- | To generate the AM signal use the math function from the Scopy signal generator. Set the main frequency | + | To generate the AM signal use the math function from the Scopy signal generator. Set the record length |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 115: | Line 115: | ||
Consider the circuit presented in Figure 9. | Consider the circuit presented in Figure 9. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 121: | Line 121: | ||
A similar circuit is added to the circuit in Figure 1 , the only difference being that the diode is reversed, allowing the negative voltages to pass through the RC circuit. | A similar circuit is added to the circuit in Figure 1 , the only difference being that the diode is reversed, allowing the negative voltages to pass through the RC circuit. | ||
- | ==== Hardware Setup: ==== | + | ==== Hardware Setup ==== |
Build the following breadboard circuit for the extended envelope detector circuit. | Build the following breadboard circuit for the extended envelope detector circuit. | ||
Line 129: | Line 129: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | === Procedure: === | + | === Procedure === |
Use the first waveform generator as source to provide the AM signal, with the following parameters: | Use the first waveform generator as source to provide the AM signal, with the following parameters: | ||
Line 136: | Line 136: | ||
* ω< | * ω< | ||
* A = 3 | * A = 3 | ||
- | To generate the AM signal use the math function from the Scopy signal generator. Set the main frequency | + | To generate the AM signal use the math function from the Scopy signal generator. Set the record length |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 166: | Line 166: | ||
2. For the circuit in Figure 1, if a resistor is added in series with the diode, between D1 and R1, how is the output affected? Explain the differences. | 2. For the circuit in Figure 1, if a resistor is added in series with the diode, between D1 and R1, how is the output affected? Explain the differences. | ||
- | ===== Further Reading | + | ===== Extra Activity: Biased Envelope Detector |
- | Additional resources: | + | The simple diode based envelope detector of Figure 1 does not well or at all if the amplitude i.e. Swing is less than the forward turn voltage of the diode. It will suffer significant distortion on the negative half of the modulation signal for high modulation indexes (near 100%) when the diode is not fully turned on. A way around this limitation is to introduce a small DC bias to the diode. This small bias current moves to quiescent operating point of the circuit to right at the turn on point of the diode. |
- | * [[http:// | + | ==== Materials ==== |
- | * [[http:// | + | |
- | * [[http:// | + | |
- | * [[http:// | + | |
- | ]] | + | |
+ | ADALM1000 Active Learning Module\\ | ||
+ | Solder-less breadboard, and jumper wire kit\\ | ||
+ | 1 - 1.5 KΩ resistor (brown green red)\\ | ||
+ | 1 - 10 KΩ resistor (brown black orange)\\ | ||
+ | 1 - 20 KΩ resistor (red black orange)\\ | ||
+ | 2 - 1.0uF capacitor, C1, C2\\ | ||
+ | 1 - 2N3904 NPN transistor\\ | ||
+ | 1 - 1N914 diode\\ | ||
+ | ==== Background ==== | ||
+ | Consider the circuit shown in Figure 14. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The amplitude modulated signal is AC coupled into the Base of NPN transistor Q1 which is configured as an emitter follower. Voltage divider R1 and R2 along with diode D1 act to set the DC bias point of the AC coupled input ([[university: | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | |||
+ | Build the following breadboard circuit for the biased envelope detector circuit. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Procedure ==== | ||
+ | |||
+ | Connect the circuit to 5V supply. | ||
+ | |||
+ | To test this circuit first use the same modulated signal you used in the simple diode envelope detector example. Compare the new design to the simple diode envelope detector. Using the same steps as earlier generate AM signals with smaller amplitudes / higher modulation indexes and compare the outputs of these two detector designs. | ||
+ | |||
+ | A plot example of the input and output waveforms for the biased envelope detector is presented in Figure 16. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ===== Further Reading ===== | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Lab Resources: | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
+ | |||
+ | Additional resources: | ||
+ | |||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | ]] | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||