This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-envelope-detector [20 Mar 2018 17:39] – [Materials] Antoniu Miclaus | university:courses:electronics:electronics-lab-envelope-detector [20 Mar 2018 17:50] – [Procedure] Antoniu Miclaus | ||
---|---|---|---|
Line 200: | Line 200: | ||
==== Procedure ==== | ==== Procedure ==== | ||
+ | |||
+ | Connect the circuit to 5V supply. | ||
To test this circuit first use the same modulated signal you used in the simple diode envelope detector example. Compare the new design to the simple diode envelope detector. Using the same steps as earlier generate AM signals with smaller amplitudes / higher modulation indexes and compare the outputs of these two detector designs. | To test this circuit first use the same modulated signal you used in the simple diode envelope detector example. Compare the new design to the simple diode envelope detector. Using the same steps as earlier generate AM signals with smaller amplitudes / higher modulation indexes and compare the outputs of these two detector designs. | ||
- | A plot example of the input and output waveforms is presented in Figure 16. | + | A plot example of the input and output waveforms |
<WRAP centeralign> | <WRAP centeralign> |