Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
university:courses:electronics:electronics-lab-envelope-detector [03 Jan 2021 22:21] – fix links Robin Getzuniversity:courses:electronics:electronics-lab-envelope-detector [10 Mar 2021 17:35] (current) – updated math equation to work with Scopy's (v1.2.0) signal generator Cristina Suteu
Line 63: Line 63:
   * ω<sub>m</sub> = 100Hz   * ω<sub>m</sub> = 100Hz
   * A = 3   * A = 3
-To generate the AM signal use the math function from the Scopy signal generator. Set the main frequency to 100Hz and apply the following function: //(1+0.5*cos(t))*3*cos(100*t)//. The generated waveform is presented in Figure 3.+To generate the AM signal use the math function from the Scopy signal generator. Set the record length to 20ms, the sample rate to 75MSPS and apply the following function: //(1+0.5*cos(2*pi*100*t))*3*cos(2*pi*100*100*t)//. The generated waveform is presented in Figure 3.
  
 <WRAP centeralign>{{:university:courses:electronics:env_detector-wgen.png|}}</WRAP> <WRAP centeralign>{{:university:courses:electronics:env_detector-wgen.png|}}</WRAP>
Line 136: Line 136:
   * ω<sub>m</sub> = 100Hz   * ω<sub>m</sub> = 100Hz
   * A = 3   * A = 3
-To generate the AM signal use the math function from the Scopy signal generator. Set the main frequency to 100Hz and apply the following function: //(1+0.5*cos(t))*3*cos(100*t)//. The generated waveform is presented in Figure 11. (with 5 displayed periods)+To generate the AM signal use the math function from the Scopy signal generator. Set the record length to 50ms and apply the following function: //(1+0.5*cos(2*pi*100*t))*3*cos(2*pi*100*100*t)//. The generated waveform is presented in Figure 11. (with 5 displayed periods)
  
 <WRAP centeralign>{{:university:courses:electronics:ext_env_detector-wgen.png|}}</WRAP> <WRAP centeralign>{{:university:courses:electronics:ext_env_detector-wgen.png|}}</WRAP>
university/courses/electronics/electronics-lab-envelope-detector.txt · Last modified: 10 Mar 2021 17:35 by Cristina Suteu