Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
university:courses:electronics:electronics-lab-ce-loop-gain [21 Jan 2020 15:20] – ↷ Links adapted because of a move operation Cristina Suteu | university:courses:electronics:electronics-lab-ce-loop-gain [26 Jan 2021 15:58] (current) – [Directions:] Doug Mercer |
---|
====Directions:==== | ====Directions:==== |
| |
Build the measurement setup as shown in figure 5 below. If you are using the HPH1-1400L transformer for T<sub>1</sub> you should connect three of the 6 windings in series for the primary and the remaining three windings in series for the secondary ( see this [[university:labs:m2k:comms_lab_transformers|activity on transformers]] for more details ). | Build the measurement setup as shown in figure 5 below. If you are using the HPH1-1400L transformer for T<sub>1</sub> you should connect three of the 6 windings in series for the primary and the remaining three windings in series for the secondary ( see this [[university:courses:alm1k:alm-lab-transformers|Transformers]] for more details ). |
| |
There are three resistors, R<sub>C</sub>, R<sub>B</sub>, R<sub>E</sub> and one capacitor, C<sub>M</sub>, that determine the loop gain of this circuit. You will be running frequency sweeps with the network analyzer testing various combinations of component values. | There are three resistors, R<sub>C</sub>, R<sub>B</sub>, R<sub>E</sub> and one capacitor, C<sub>M</sub>, that determine the loop gain of this circuit. You will be running frequency sweeps with the network analyzer testing various combinations of component values. |
<WRAP round download> | <WRAP round download> |
**Resources:** | **Resources:** |
* LTSpice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/ltspice/ce_loop_gain_ltspice | ce_loop_gain_ltspice]] | * LTSpice files: [[downgit>education_tools/tree/master/m2k/ltspice/ce_loop_gain_ltspice | ce_loop_gain_ltspice]] |
</WRAP> | </WRAP> |
| |