university:courses:electronics:electronics-lab-capacitors [08 Feb 2013 21:05]
Doug Mercer [CAPACITOR COMPARISON CHART]
university:courses:electronics:electronics-lab-capacitors [03 Jan 2021 22:21] (current)
Robin Getz fix links
Line 44: Line 44:
 Electrolytic capacitors are polarized and **they must be connected with the correct orientation**,​ at least one of their leads will be marked with a + or -. They are not generally damaged by heat when soldering but can overheat and be damaged if connected with the wrong polarity. Electrolytic capacitors are polarized and **they must be connected with the correct orientation**,​ at least one of their leads will be marked with a + or -. They are not generally damaged by heat when soldering but can overheat and be damaged if connected with the wrong polarity.
    
-There are two designs of electrolytic capacitors; **axial** where the leads are attached to each end (220µF in picture) ​and **radial** where both leads are at the same end (10µF in picture). Radial capacitors tend to be a little smaller and they stand upright on the circuit board.+There are two designs of electrolytic capacitors; **axial** where the leads are attached to each end and **radial** where both leads are at the same end. Radial capacitors tend to be a little smaller and they stand upright on the circuit board while axial capacitors can have a lower profile on a PC board but may take up more space.
    
 {{ :​university:​courses:​electronics:​acap_f4.png?​100 |}} {{ :​university:​courses:​electronics:​acap_f4.png?​100 |}}
Line 295: Line 295:
 ==== For more info on passive components see: ==== ==== For more info on passive components see: ====
  
-[[http://​www.analog.com/​static/​imported-files/​application_notes/​500824934643930414583807523874018494695982855668424783486554001060AN348.pdf|AN-348:​ Avoiding Passive-Component Pitfalls]]+[[adi>static/​imported-files/​application_notes/​500824934643930414583807523874018494695982855668424783486554001060AN348.pdf|AN-348:​ Avoiding Passive-Component Pitfalls]]
  
 **Return to Lab Activities [[university:​courses:​electronics:​labs|Table of Contents]]** **Return to Lab Activities [[university:​courses:​electronics:​labs|Table of Contents]]**
  
  
university/courses/electronics/electronics-lab-capacitors.1360353924.txt.gz · Last modified: 08 Feb 2013 21:05 by Doug Mercer