This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-capacitors [24 Jan 2013 21:12] – created Doug Mercer | university:courses:electronics:electronics-lab-capacitors [17 Jun 2013 14:45] – minor edit to remove picture reference Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Capacitors ====== | + | ====== |
===== Function: ===== | ===== Function: ===== | ||
Line 34: | Line 34: | ||
Examples: | Examples: | ||
- | {{: | + | {{: |
Circuit Symbol: | Circuit Symbol: | ||
Line 44: | Line 44: | ||
Electrolytic capacitors are polarized and **they must be connected with the correct orientation**, | Electrolytic capacitors are polarized and **they must be connected with the correct orientation**, | ||
- | There are two designs of electrolytic capacitors; **axial** where the leads are attached to each end (220µF in picture) | + | There are two designs of electrolytic capacitors; **axial** where the leads are attached to each end and **radial** where both leads are at the same end. Radial capacitors tend to be a little smaller and they stand upright on the circuit board while axial capacitors can have a lower profile on a PC board but may take up more space. |
{{ : | {{ : | ||
Line 54: | Line 54: | ||
Tantalum bead capacitors are polarized and have low voltage ratings similar to electrolytic capacitors. They can be more expensive but are very small, so they are used where a large capacitance is needed in a small space. | Tantalum bead capacitors are polarized and have low voltage ratings similar to electrolytic capacitors. They can be more expensive but are very small, so they are used where a large capacitance is needed in a small space. | ||
- | {{ : | + | {{ : |
Modern tantalum bead capacitors are printed with their capacitance and voltage in full. However older ones use a color-code system which has two stripes (for the two digits) and a spot of color for the number of zeros to give the value in µF. The standard color code is used, but for the spot, **grey** is used to mean × 0.01 and **white** means × 0.1 so that values of less than 10µF can be shown. A third color stripe near the leads shows the voltage (yellow 6.3V, black 10V, green 16V, blue 20V, grey 25V, white 30V, pink 35V). | Modern tantalum bead capacitors are printed with their capacitance and voltage in full. However older ones use a color-code system which has two stripes (for the two digits) and a spot of color for the number of zeros to give the value in µF. The standard color code is used, but for the spot, **grey** is used to mean × 0.01 and **white** means × 0.1 so that values of less than 10µF can be shown. A third color stripe near the leads shows the voltage (yellow 6.3V, black 10V, green 16V, blue 20V, grey 25V, white 30V, pink 35V). | ||
Line 65: | Line 65: | ||
Examples: | Examples: | ||
- | {{: | + | {{: |
+ | {{: | ||
Circuit symbol: | Circuit symbol: | ||
Line 225: | Line 226: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
Stray or “parasitic” capacitance commonly occurs between parallel traces on a PC board or between traces/ | Stray or “parasitic” capacitance commonly occurs between parallel traces on a PC board or between traces/ | ||
Line 291: | Line 292: | ||
| Aluminum electrolytic | High | Large values High currents High voltages Small size | High leakage Usually polarized Poor stability Poor accuracy Inductive | | | Aluminum electrolytic | High | Large values High currents High voltages Small size | High leakage Usually polarized Poor stability Poor accuracy Inductive | | ||
| Tantalum electrolytic | High | Small size Large values Medium inductance | Quite high leakage Usually polarized Expensive Poor stability Poor accuracy | | | Tantalum electrolytic | High | Small size Large values Medium inductance | Quite high leakage Usually polarized Expensive Poor stability Poor accuracy | | ||
+ | |||
+ | ==== For more info on passive components see: ==== | ||
+ | |||
+ | [[http:// | ||
**Return to Lab Activities [[university: | **Return to Lab Activities [[university: | ||