Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:electronics-lab-breadboard-coupling [12 Apr 2017 12:40]
amiclaus rename
university:courses:electronics:electronics-lab-breadboard-coupling [24 Jul 2017 14:58] (current)
amiclaus change amplitude value to peak-peak
Line 48: Line 48:
 ===== Hardware Setup: ===== ===== Hardware Setup: =====
  
-Using the Network Analyzer instrument in the Scopy software obtain a gain (attenuation) vs. frequency plot from 10 Hz to 10 MHz. Scope channel 1 is the "​filter"​ input and scope channel 2 is the "​filter"​ output. Set AWG offset to 0 and the Amplitude to 1V with the Max-Gain set to 0.1X. Set the vertical scale to start at 1dB with an 80 dB range. Run a single sweep and export the data to a .csv file.+Using the Network Analyzer instrument in the Scopy software obtain a gain (attenuation) vs. frequency plot from 10 Hz to 10 MHz. Scope channel 1 is the "​filter"​ input and scope channel 2 is the "​filter"​ output. Set AWG offset to 0 and the Amplitude to 2V with the Max-Gain set to 0.1X. Set the vertical scale to start at 1dB with an 80 dB range. Run a single sweep and export the data to a .csv file.
  
 ===== Procedure: ===== ===== Procedure: =====
university/courses/electronics/electronics-lab-breadboard-coupling.txt · Last modified: 24 Jul 2017 14:58 by amiclaus