This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-9 [05 Mar 2019 12:24] – [Using an NPN transistor array:] Antoniu Miclaus | university:courses:electronics:electronics-lab-9 [05 Nov 2021 15:28] (current) – [Activity: Regulated Voltage Reference] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: |
====== Version 1 ====== | ====== Version 1 ====== | ||
Line 5: | Line 5: | ||
===== Objective: ===== | ===== Objective: ===== | ||
- | The zero gain amplifier (Q< | + | The zero gain amplifier (Q< |
===== Materials: ===== | ===== Materials: ===== | ||
Line 29: | Line 29: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Waveform generator 1 should be configured for a 1 KHz triangle wave with 4 volt amplitude and 2V offset. The Single ended input of scope channel 2 (2+) is used to measure the stabilized output voltage at the collector of Q< | + | Waveform generator 1 should be configured for a 1 KHz triangle wave with 4 volt amplitude |
===== Procedure: ===== | ===== Procedure: ===== | ||
Line 66: | Line 66: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Waveform generator W1 should be configured for a 1 KHz triangle wave with 4 volt amplitude and 2V offset. Scope channel 2 (2+) is used to measure the stabilized output voltage at the emitter of Q< | + | Waveform generator W1 should be configured for a 1 KHz triangle wave with 4 volt amplitude |
===== Procedure: ===== | ===== Procedure: ===== | ||
Line 78: | Line 78: | ||
==== For Further Study: ==== | ==== For Further Study: ==== | ||
- | ADI Mini Tutorial on [[http:// | + | ADI Mini Tutorial on [[adi>static/ |
====== Using an NPN transistor array: ====== | ====== Using an NPN transistor array: ====== | ||
Line 90: | Line 90: | ||
<WRAP round download> | <WRAP round download> | ||
**Resources: | **Resources: | ||
- | * Fritzing files: [[ https:// | + | * Fritzing files: [[downgit>education_tools/ |
- | * LTspice files: [[ https:// | + | * LTspice files: [[downgit>education_tools/ |
</ | </ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||