Next revision Both sides next revision
university:courses:electronics:electronics-lab-9 [05 Mar 2019 12:24]
Antoniu Miclaus [Using an NPN transistor array:]
university:courses:electronics:electronics-lab-9 [23 Aug 2019 13:05]
Antoniu Miclaus
Line 1: Line 1:
-====== Activity ​9.  ​Regulated Voltage Reference ======+====== Activity ​Regulated Voltage Reference ======
  
 ====== Version 1 ====== ====== Version 1 ======
Line 5: Line 5:
 ===== Objective: ===== ===== Objective: =====
  
-The zero gain amplifier (Q<​sub>​1</​sub>,​ R<​sub>​2</​sub>​) and stabilized current source (Q<​sub>​2</​sub>,​ R<​sub>​3</​sub>​) from activities ​and can be used in conjunction with a PNP current mirror stage (Q<​sub>​3</​sub>,​Q<​sub>​4</​sub>​) in negative feedback to build a circuit which provides a constant or regulated output voltage over a range of input voltages.+The zero gain amplifier (Q<​sub>​1</​sub>,​ R<​sub>​2</​sub>​) and stabilized current source (Q<​sub>​2</​sub>,​ R<​sub>​3</​sub>​) from activities ​10 and 11 can be used in conjunction with a PNP current mirror stage (Q<​sub>​3</​sub>,​Q<​sub>​4</​sub>​) in negative feedback to build a circuit which provides a constant or regulated output voltage over a range of input voltages.
  
 ===== Materials: ===== ===== Materials: =====
Line 29: Line 29:
 <WRAP centeralign>​ Figure 2 Regulator Version 1 Breadboard Circuit </​WRAP>​ <WRAP centeralign>​ Figure 2 Regulator Version 1 Breadboard Circuit </​WRAP>​
  
-Waveform generator 1 should be configured for a 1 KHz triangle wave with 4 volt amplitude and 2V offset. The Single ended input of scope channel 2 (2+) is used to measure the stabilized output voltage at the collector of Q<​sub>​4</​sub>​ ( negative inputs 1= and 2- should be connected to ground).+Waveform generator 1 should be configured for a 1 KHz triangle wave with 4 volt amplitude ​peak-to-peak ​and 2V offset. The Single ended input of scope channel 2 (2+) is used to measure the stabilized output voltage at the collector of Q<​sub>​4</​sub>​ ( negative inputs 1= and 2- should be connected to ground).
  
 ===== Procedure: ===== ===== Procedure: =====
Line 66: Line 66:
 <WRAP centeralign>​ Figure 5 Regulator Version 2 Breadboard Circuit</​WRAP>​ <WRAP centeralign>​ Figure 5 Regulator Version 2 Breadboard Circuit</​WRAP>​
  
-Waveform generator W1 should be configured for a 1 KHz triangle wave with 4 volt amplitude and 2V offset. Scope channel 2 (2+) is used to measure the stabilized output voltage at the emitter of Q<​sub>​4</​sub>​.+Waveform generator W1 should be configured for a 1 KHz triangle wave with 4 volt amplitude ​peak-to-peak ​and 2V offset. Scope channel 2 (2+) is used to measure the stabilized output voltage at the emitter of Q<​sub>​4</​sub>​.
  
 ===== Procedure: ===== ===== Procedure: =====
university/courses/electronics/electronics-lab-9.txt · Last modified: 05 Nov 2021 15:28 by Doug Mercer