Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
university:courses:electronics:electronics-lab-8m [05 Mar 2019 12:24]
Antoniu Miclaus [Questions:]
university:courses:electronics:electronics-lab-8m [23 Aug 2019 12:54]
Antoniu Miclaus
Line 1: Line 1:
-====== Activity ​8M. Stabilized current source (NMOS) ======+====== ActivityStabilized current source (NMOS) ======
  
 ===== Objective: ===== ===== Objective: =====
Line 28: Line 28:
 <WRAP centeralign>​ Figure 2 Stabilized current source Breadboard Circuit </​WRAP>​ <WRAP centeralign>​ Figure 2 Stabilized current source Breadboard Circuit </​WRAP>​
  
-The waveform generator should be configured for a 1 KHz triangle wave with 4 volt amplitude and 2V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the drain of M<​sub>​2</​sub>​.+The waveform generator should be configured for a 1 KHz triangle wave with 4 volt amplitude ​peak-to-peak ​and 2V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the drain of M<​sub>​2</​sub>​.
    
 ===== Procedure:​===== ===== Procedure:​=====
university/courses/electronics/electronics-lab-8m.txt · Last modified: 25 Jun 2020 22:07 (external edit)