This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-8m [12 Jul 2019 13:24] – [Activity 8M. Stabilized current source (NMOS)] Pop Andreea | university:courses:electronics:electronics-lab-8m [23 Aug 2019 12:54] – Antoniu Miclaus | ||
---|---|---|---|
Line 28: | Line 28: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | The waveform generator should be configured for a 1 KHz triangle wave with 4 volt amplitude and 2V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the drain of M< | + | The waveform generator should be configured for a 1 KHz triangle wave with 4 volt amplitude |
===== Procedure: | ===== Procedure: |