This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-8a [05 Mar 2019 12:24] – [Questions:] Antoniu Miclaus | university:courses:electronics:electronics-lab-8a [20 Jul 2022 20:35] (current) – [Objective:] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: A Floating (two terminal) Current Source / Sink ====== |
- | ===== Objective: ===== | + | =====Objective: |
The objective of this activity is to investigate the ΔV< | The objective of this activity is to investigate the ΔV< | ||
+ | =====Background: | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | The AD590 uses a fundamental property of silicon BJT transistors to realize its temperature proportional characteristic. If two identical transistors are operated at a constant ratio of collector current densities, r, then the difference in their base-emitter voltage is (kT/q)(In r). Because both k (Boltzman’s constant) and q (the charge of an electron) are constant, the resulting voltage is directly proportional to absolute temperature (PTAT). For more details please refer to the datasheet. | ||
===== Materials: ===== | ===== Materials: ===== | ||
ADALM2000 Active Learning Module\\ | ADALM2000 Active Learning Module\\ | ||
Line 33: | Line 38: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Configure waveform generator AWG1 as a triangle wave with a frequency of 100 Hz and an amplitude of 10 V with 0 V offset. The scope display should be set in both voltage vs. time and in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis. Be sure to turn on the power supply only after you have completed and double checked your connections. | + | Configure waveform generator AWG1 as a triangle wave with a frequency of 100 Hz and an amplitude of 10 V peak-to-peak |
===== Procedure: ===== | ===== Procedure: ===== | ||
Line 51: | Line 56: | ||
===== Prove the floating nature of circuit: ===== | ===== Prove the floating nature of circuit: ===== | ||
- | In figure 1 we referenced the negative end of the circuit to a negative power supply. To prove that this circuit is truly a floating current source, rearrange your breadboard to look like figure | + | In figure 1 we referenced the negative end of the circuit to a negative power supply. To prove that this circuit is truly a floating current source, rearrange your breadboard to look like figure |
{{ : | {{ : | ||
Line 75: | Line 80: | ||
<WRAP round download> | <WRAP round download> | ||
**Resources: | **Resources: | ||
- | * Fritzing files: [[ https:// | + | * Fritzing files: [[downgit>education_tools/ |
- | * LTspice files: [[ https:// | + | * LTspice files: [[downgit>education_tools/ |
</ | </ | ||