Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Last revisionBoth sides next revision
university:courses:electronics:electronics-lab-8 [12 Jul 2019 13:24] – [Activity 8. Stabilized current source (BJT)] Pop Andreeauniversity:courses:electronics:electronics-lab-8 [23 Aug 2019 12:53] Antoniu Miclaus
Line 28: Line 28:
 <WRAP centeralign> Figure 2 Stabilized current source Breadboard Circuit </WRAP> <WRAP centeralign> Figure 2 Stabilized current source Breadboard Circuit </WRAP>
  
-The waveform generator should be configured for a 1 KHz triangle wave with 3 volt amplitude and 1.5V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the collector of Q2.+The waveform generator should be configured for a 1 KHz triangle wave with 3 volt amplitude peak-to-peak and 1.5V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the collector of Q2.
  
 ===== Procedure: ===== ===== Procedure: =====
university/courses/electronics/electronics-lab-8.txt · Last modified: 25 Jun 2020 22:07 by 127.0.0.1