This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-8 [28 Oct 2012 19:32] – created Doug Mercer | university:courses:electronics:electronics-lab-8 [23 Aug 2019 12:53] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: Stabilized current source (BJT) ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 7: | Line 7: | ||
===== Materials: ===== | ===== Materials: ===== | ||
- | Analog Discovery Lab hardware\\ | + | ADALM2000 Active Learning Module\\ |
Solder-less breadboard\\ | Solder-less breadboard\\ | ||
1 - 2.2KΩ Resistor ( or any similar value )\\ | 1 - 2.2KΩ Resistor ( or any similar value )\\ | ||
Line 24: | Line 24: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 1 KHz triangle wave with 1.5 volt amplitude and 1.5V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the collector of Q2. | + | {{: |
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The waveform generator should be configured for a 1 KHz triangle wave with 3 volt amplitude | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
The zero gain amplifier can be used to create a stabilized current source. Because the voltage seen at the collector of transistor Q< | The zero gain amplifier can be used to create a stabilized current source. Because the voltage seen at the collector of transistor Q< | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | **Resources: | ||
+ | * LTSpice files: [[ https:// | ||
===== Questions: ===== | ===== Questions: ===== | ||
Line 40: | Line 55: | ||
Based on the delta V< | Based on the delta V< | ||
- | An exercise for the student | + | An exercise for the reader |
The output of the simple peaking current source is always less than the input current at the peak by a substantial fraction. What is that fraction and why? | The output of the simple peaking current source is always less than the input current at the peak by a substantial fraction. What is that fraction and why? | ||
Line 47: | Line 62: | ||
The output current has a narrow peak. How could multiple copies of the peaking current source be combined to produce a much wider, flatter peak? | The output current has a narrow peak. How could multiple copies of the peaking current source be combined to produce a much wider, flatter peak? | ||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * Fritzing files: [[ https:// | ||
+ | * LTspice files: [[ https:// | ||
+ | </ | ||
+ | |||
+ | **Return to Lab Activity [[university: | ||