This shows you the differences between two versions of the page.
Next revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-7m [28 Oct 2012 19:28] – created Doug Mercer | university:courses:electronics:electronics-lab-7m [23 Aug 2019 12:53] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: Zero gain amplifier (MOS) ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 8: | Line 8: | ||
===== Materials :===== | ===== Materials :===== | ||
- | Analog Discovery Lab hardware\\ | + | ADALM2000 Active Learning Module\\ |
Solder-less breadboard\\ | Solder-less breadboard\\ | ||
1 - 2.2KΩ Resistor (or any similar value)\\ | 1 - 2.2KΩ Resistor (or any similar value)\\ | ||
Line 24: | Line 24: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator 1 should be configured for a 1 KHz triangle wave with 2 volt amplitude and 2V offset. Connect scope Channel 1 to display output W1 of the AWG generator. The Single ended input of scope channel 2 (2+) is used to measure alternately the gate and drain voltage of M< | + | {{: |
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The waveform generator 1 should be configured for a 1 KHz triangle wave with 4 volt amplitude | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
Line 31: | Line 35: | ||
In the figure below we have a transistor biased into saturation region with a drain voltage which is less than the gate voltage by , (equal to I< | In the figure below we have a transistor biased into saturation region with a drain voltage which is less than the gate voltage by , (equal to I< | ||
- | {{ : | + | <WRAP centeralign> |
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
===== Questions: ===== | ===== Questions: ===== | ||
Line 41: | Line 51: | ||
What are the relative gains of the two paths when the drain current is less than and greater than the " | What are the relative gains of the two paths when the drain current is less than and greater than the " | ||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * Fritzing files: [[ https:// | ||
+ | * LTspice files: [[ https:// | ||
+ | </ | ||
+ | **Return to Lab Activity [[university: | ||