Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
university:courses:electronics:electronics-lab-6m [12 Jul 2019 13:22] – Pop Andreea | university:courses:electronics:electronics-lab-6m [25 Jun 2020 22:07] (current) – external edit 127.0.0.1 |
---|
===== Hardware Setup: ===== | ===== Hardware Setup: ===== |
| |
In the current mirror configuration, the opamp serves as a virtual ground at the mirror input (gate) node to convert the voltage steps from AWG 1 ( W1 output ) into current steps through the 1K? resistor. The drain voltage is swept using a ramp from AWG 1(output W1). Load the stairstep.csv file, set amplitude to 1.5 (3V peak to peak) with the offset to 1.5V. | In the current mirror configuration, the opamp serves as a virtual ground at the mirror input (gate) node to convert the voltage steps from AWG 1 ( W1 output ) into current steps through the 1K? resistor. The drain voltage is swept using a ramp from AWG 1(output W1). Load the stairstep.csv file, set amplitude to 3V peak-to-peak with the offset to 1.5V. |
V<sub>DS</sub> of output device M<sub>2</sub> is measured differentially by scope inputs 1+, 1-. The mirror output current is measured by scope inputs 2+. 2- across 1K? resistor, R<sub>2</sub>. | V<sub>DS</sub> of output device M<sub>2</sub> is measured differentially by scope inputs 1+, 1-. The mirror output current is measured by scope inputs 2+. 2- across 1K? resistor, R<sub>2</sub>. |
If you don't want to use the op-amp configuration the following simplified configuration can be used as well. | If you don't want to use the op-amp configuration the following simplified configuration can be used as well. |
<WRAP round download> | <WRAP round download> |
**Resources:** | **Resources:** |
* Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/mos_current_mirror_bb | mos_current_mirror_bb]] | * Fritzing files: [[downgit>education_tools/tree/master/m2k/fritzing/mos_current_mirror_bb | mos_current_mirror_bb]] |
* LTspice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/ltspice/nmos_cur_mirror_ltspice | mos_current_mirror_ltspice]] | * LTspice files: [[downgit>education_tools/tree/master/m2k/ltspice/nmos_cur_mirror_ltspice | mos_current_mirror_ltspice]] |
</WRAP> | </WRAP> |
===== Questions: ===== | ===== Questions: ===== |