Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:electronics-lab-6 [12 Jul 2019 13:06]
Pop Andreea
university:courses:electronics:electronics-lab-6 [23 Aug 2019 12:50]
Antoniu Miclaus
Line 30: Line 30:
 ===== Hardware Setup: ===== ===== Hardware Setup: =====
  
-In the current mirror configuration,​ the op amp serves as a virtual ground at the mirror input (base) node to convert the voltage steps from AWG 2 ( W2 output ) into current steps through the 1KΩ resistor. The collector voltage is swept using a ramp from AWG 1(output W1). Load the stairstep.csv file, set amplitude to 1.5  (3V peak to peakwith the offset to 1.5V. +In the current mirror configuration,​ the op amp serves as a virtual ground at the mirror input (base) node to convert the voltage steps from AWG 2 ( W2 output ) into current steps through the 1KΩ resistor. The collector voltage is swept using a ramp from AWG 1(output W1). Load the stairstep.csv file, set amplitude to 3V peak-to-peak with the offset to 1.5V. 
 V<​sub>​CE</​sub>​ of output device Q<​sub>​2</​sub>​ is measured differentially by scope inputs 1+, 1-. The mirror output current is measured by scope inputs 2+. 2- across 1KΩ resistor, R<​sub>​2</​sub>​. V<​sub>​CE</​sub>​ of output device Q<​sub>​2</​sub>​ is measured differentially by scope inputs 1+, 1-. The mirror output current is measured by scope inputs 2+. 2- across 1KΩ resistor, R<​sub>​2</​sub>​.
 If you don't want to use the op-amp configuration the following simplified configuration can be used as well. If you don't want to use the op-amp configuration the following simplified configuration can be used as well.
university/courses/electronics/electronics-lab-6.txt · Last modified: 25 Jun 2020 22:07 (external edit)