Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:electronics-lab-5m [12 Jul 2019 13:04]
andreeapop
university:courses:electronics:electronics-lab-5m [23 Aug 2019 12:40] (current)
amiclaus
Line 23: Line 23:
 ===== Hardware Setup: ===== ===== Hardware Setup: =====
  
-The waveform generator W1 should be configured for a 1 KHz Sine wave with 3 volt amplitude and 0 volt offset. The setup should be configured with scope channel 1+ connected to display the output W1. Scope channel 2 (2+) is used to measure alternately the waveform at the gate and drain of M<​sub>​1</​sub>​.+The waveform generator W1 should be configured for a 1 KHz Sine wave with 3 volt amplitude ​peak-to-peak ​and 0 volt offset. The setup should be configured with scope channel 1+ connected to display the output W1. Scope channel 2 (2+) is used to measure alternately the waveform at the gate and drain of M<​sub>​1</​sub>​.
 {{ :​university:​courses:​electronics:​a5m_nf2.png?​ |}} {{ :​university:​courses:​electronics:​a5m_nf2.png?​ |}}
  
university/courses/electronics/electronics-lab-5m.txt · Last modified: 23 Aug 2019 12:40 by amiclaus