Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:electronics:electronics-lab-5 [12 Jul 2019 13:02]
andreeapop
university:courses:electronics:electronics-lab-5 [23 Aug 2019 12:40] (current)
amiclaus
Line 25: Line 25:
 <WRAP centeralign>​ Figure 2 Common emitter amplifier test configuration breadboard connection </​WRAP>​ <WRAP centeralign>​ Figure 2 Common emitter amplifier test configuration breadboard connection </​WRAP>​
  
-The waveform generator output W1 should be configured for a 1 KHz sine wave with 3 volt amplitude and 0 volt offset. The setup should be configured with scope channel 1+ connected to display the output W1. Scope channel 2 (2+) is used to measure alternately the waveform at the base and collector of Q<​sub>​1</​sub>​.+The waveform generator output W1 should be configured for a 1 KHz sine wave with 3 volt amplitude ​peak-to-peak ​and 0 volt offset. The setup should be configured with scope channel 1+ connected to display the output W1. Scope channel 2 (2+) is used to measure alternately the waveform at the base and collector of Q<​sub>​1</​sub>​.
  
 ===== Procedure: ===== ===== Procedure: =====
university/courses/electronics/electronics-lab-5.txt · Last modified: 23 Aug 2019 12:40 by amiclaus